cancel
Showing results for 
Search instead for 
Did you mean: 

Does NUCLEO-L4R5ZI-P board support Hyperbus Protocol?

AGEBE.1
Associate II

I saw that Hyperbus protocol with differential clock (1.8V) is not available on STM3L4R5ZIT6P, but Hyperbus protocol with single-ended clock(3.3V) is.

My question is : is the Nucleo -L4R5ZI-P board supporting Hyperbus protocol with single-ended clock because I haven’t seen any reference to it in NUCLEO’s documentation?

Thanks

1 REPLY 1

The NUCLEO provide little in the way of on board hardware. You should check the data manual for pin usages, and reference manual for the chip level support. You'll need to code drivers, or find some​ to back port.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..