2019-09-06 3:49 AM
Does exist in the current datasheet (April 2019 Rev 7) different information about the pinning regarding the alphabetic ordered rows for the TFBGA240+25 package? In chapter 5 Pin descriptions the rows starts with letter "A" and ends with letter "U". In chapter 8.8 TFBGA240+25 package information the rows starts with the letter "A" and ends with letter "S". What is correct right now ? I am a little confused. But this information is absolutely relevant to know the right pinning.
Please see attachments. There are Screenshots from the datasheet.
Thanks beforehand for your help.
BR
Wolfgang
2019-09-10 6:56 AM
It seems not much people are busy with the current footprint ;)
2019-09-10 8:18 AM
I usually resolve similar errors by... voting. :D No, but serious, look for other sources of the same information. In this case look at pin descriptions for that package - they're all "U" based and there is none with "S". :)
P.S. Of course it's still an error and needs fixing.
2019-09-10 11:29 PM
@Piranha Thanks. It seems it helps only your advice. I will take it so...
2019-09-26 4:20 AM
Hi @WWalt.1 ,
I join @Piranha to confirm that "U" is the correct marking; we can confirm it based on the pins naming on pinout table for the column TFBGA240+25.
The marking in the figure "TFBGA240+25 package outline" will be fixed on all relevant datasheets.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.