2019-12-19 03:21 PM
Hi,
This is what I found in the reference manual:
Once the transfer is completed, this [NDT] register can either stay at zero (when the stream is in normal mode) or be reloaded automatically with the previously programmed value in the following cases:
– when the stream is configured in circular mode.
– when the stream is enabled again by setting EN bit to '1'.
What I understand is, that in circular mode after each transfer the NDT register gets reloaded (which makes obviously sense).
But what happens in the following situations (for non-circular streams):
I hope this question isn't that stupid
Answers are really appreciated.
Solved! Go to Solution.
2019-12-19 10:59 PM
NDTR is not one register but two: one into which you write, and a second one, which you read, let's denote them NDTR_W and NDTR_R.
When DMA is enabled, NDTR_W is copied into NDTR_R and then governs the rest of the DMA process. As long as you don't overwrite NDTR_W, every subsequent enable (or "recycle" in circular mode) uses the same, last-written, value from NDTR_W to copy into NDTR_R.
(Btw., the pointer registers are also doubled, but in a different way - there's a read-write register, which does not participate in DMA process except that its content is copied into its "invisible working" counterpart when the channel/stream is enabled/recycled.)
The net effective result is, that you cannot continue an aborted transfer without rewriting the registers, and that also means that you cannot abort/continue a circular transfer at all.
JW
2019-12-19 10:59 PM
NDTR is not one register but two: one into which you write, and a second one, which you read, let's denote them NDTR_W and NDTR_R.
When DMA is enabled, NDTR_W is copied into NDTR_R and then governs the rest of the DMA process. As long as you don't overwrite NDTR_W, every subsequent enable (or "recycle" in circular mode) uses the same, last-written, value from NDTR_W to copy into NDTR_R.
(Btw., the pointer registers are also doubled, but in a different way - there's a read-write register, which does not participate in DMA process except that its content is copied into its "invisible working" counterpart when the channel/stream is enabled/recycled.)
The net effective result is, that you cannot continue an aborted transfer without rewriting the registers, and that also means that you cannot abort/continue a circular transfer at all.
JW