cancel
Showing results for 
Search instead for 
Did you mean: 

Distinguish different STM32G0 variants at run-time

TR01
Associate

Hi,
Is it possible to distinguish an STM32G0B1KBU6N from an STM32G0B1KBU6 based on the UID?
Is it possible to read this UID in FW in order to recognize whether the correct controller is fitted or is this only possible via the SW interface?

4 REPLIES 4
Pavel A.
Evangelist III

There's  some register (or ROM location) that tells the package type.

 


@TR01 wrote:

Is it possible to read this UID in FW 


Yes - see:

https://community.st.com/t5/stm32-mcus/how-to-obtain-and-use-the-stm32-96-bit-uid/ta-p/621443

 


@TR01 wrote:

Is it possible to distinguish an STM32G0B1KBU6N from an STM32G0B1KBU6 based on the UID?


It doesn't look like it.

As @Pavel A. said, there may be other ROM locations which may help ...

 

These part numbers STM32G0B1KBU6N and STM32G0B1KBU6 difference is the N at the end, UID, Flash size and package information don't give this differentiation. 

SofLit_0-1727878430318.png

So I don't think it's possible to get that information by software.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.