cancel
Showing results for 
Search instead for 
Did you mean: 

My USB-C Nucelo boards cannot detect ST-Link

kag_embedded
Associate III

I just received a NUCLEO-H503RB dev board, and while attempting to use the GPIO_IOToggle example program to test out the board, I could not run the debugger due to the error "ST-Link not detected." I went back to my NUCLEO-H7S3L8 board, it now receives the same error. A few days ago, I was able to program it.


I was able to detect the ST-Link with my NUCLEO-F446RE board.


Do I need to reinstall ST-Link or is there a way to force a firmware update on my two NUCLEO USBC dev kits?

 

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions
kag_embedded
Associate III

Trying a 3rd cable was the key. It is quite touchy on the USBC cable.
With the 3rd cable, it shows up on my Device Manager and I can connect to it via STM32cubeIDE.
I am considering this issue resolved. Thank you for your help.

View solution in original post

13 REPLIES 13
Chris21
Senior III

Are you using the correct USB connector? 

Labeled USB STLK.

I have tried both USBC ports. One port, the LEDs do not light up. The other USBC port, near the header pins with the ST-LINK pins which are shorted together, blink through what appears to be a boot up sequence and then LED3 blinks at a regular pulse rate.

What should I try next?

Thank you.

Chris21
Senior III

Not sure, my NUCLEO-H503RB worked immediately. 

"the header pins with the ST-LINK pins which are shorted together"?

Which pins are those?  JP1 should not have a jumper.

JP5, SW_STLK pins are shorted to +5v.

5V_STLK shorted to +5V is the normal use case, board powered from ST-LINK USB connector.

What should I try next?

Is there a way to force a refresh of the NUCLEO's firmware? On the Silicon Labs kits, you can force an update of the firmware in situations similar to this.

 

kag_embedded
Associate III

Would using JP1 to reset the STLNK be worth a try? If yes, do I just short it out and then remove the short?

I believe STM32CubeProgrammer can be used to reprogram the ST-LINK, but I have not needed to do that.

"do I just short it out and then remove the short?"  

That will reset the ST-LINK MCU, I don't expect it will solve your problem, though.