2022-10-26 4:07 AM
I'm stuck trying to understand the differences between the two Nucleo-144 boards
STM32H743ZI (seems to be the older version but with lots of resources but outdated)
and
STM32H743ZI2 (current version but i can hardly find working examples and resources)
can someone point me in the right direction?
why do some examples designed for the ZI not work on the ZI2 ?
where exactly are the diferences, at first glance they seem identical.
Solved! Go to Solution.
2022-10-26 10:47 AM
Related defines, check stm32h7xx_nucleo_conf.h
USE_HAL_DRIVER, STM32H743xx, USE_NUCLEO_144
USE_NUCLEO_H743ZI
USE_NUCLEO_H743ZI2
LED2
PB7 BLUE (ZI)
PE1 YELLOW (ZI2)
ARDUINO D4
PF14 (ZI)
PE14 (ZI2)
ARDUINO D8
PG9 (ZI)
PF3 (ZI2)
PE2 QSPI/SAI CONFLICTED
PB13 SAI/ETHERNET CONFLICTED
PA7 D11/ETHERNET CONFLICTED
QSPI CS
PB6 (ZI)
PG6 (ZI2) or PB6 will SB made
Read the notes and solder-bridge options/defaults
MB1137 UM1974 (ZI)
https://www.st.com/resource/en/schematic_pack/nucleo_144pins_sch.zip
MB1364 UM2407 (ZI2)
2022-10-26 4:46 AM
Handful of pins related to LEDs, QSPI and ETHERNET, as I recall, reducing/removing some potential stubs. Solder Bridges and default usage expectations.
Different HSE clock furnished by ST-LINK/V3
2022-10-26 6:36 AM
could you go ito detail about the ethernet pins particularly? where did you find documentation that explains that?
2022-10-26 7:06 AM
2022-10-26 7:14 AM
I went through the manual and schematic whilst porting some QSPI support.
Perhaps start by looking at the MORPHO connector.
2022-10-26 10:47 AM
Related defines, check stm32h7xx_nucleo_conf.h
USE_HAL_DRIVER, STM32H743xx, USE_NUCLEO_144
USE_NUCLEO_H743ZI
USE_NUCLEO_H743ZI2
LED2
PB7 BLUE (ZI)
PE1 YELLOW (ZI2)
ARDUINO D4
PF14 (ZI)
PE14 (ZI2)
ARDUINO D8
PG9 (ZI)
PF3 (ZI2)
PE2 QSPI/SAI CONFLICTED
PB13 SAI/ETHERNET CONFLICTED
PA7 D11/ETHERNET CONFLICTED
QSPI CS
PB6 (ZI)
PG6 (ZI2) or PB6 will SB made
Read the notes and solder-bridge options/defaults
MB1137 UM1974 (ZI)
https://www.st.com/resource/en/schematic_pack/nucleo_144pins_sch.zip
MB1364 UM2407 (ZI2)