cancel
Showing results for 
Search instead for 
Did you mean: 

difference between real measured frequency and set frequency

PetrK
Associate II

Hello,

I am dealing with difference between real measured frequency and set on my Nucleo H755ZI-Q.
the measured real frequency :
APB1 76,8 MHz
APB2 76,8 MHz
recalculated
debugging frequencz SWV Core Clock 153,6 MHz

I also try printf debuged frequency:
HSE is enabled and ready.
System Clock: 480000000 Hz
APB1 Timer Clock: 120000000 Hz
APB2 Timer Clock: 120000000 Hz
APB1 Prescaler: 4
APB2 Prescaler: 4
PetrK_0-1744104643584.png

if ((RCC->CR & RCC_CR_HSERDY) != 0) { printf("HSE is enabled and ready.\n"); } else { printf("HSE is not enabled or ready.\n"); } printf("System Clock: %lu Hz\n", HAL_RCC_GetSysClockFreq()); printf("APB1 Timer Clock: %lu Hz\n", HAL_RCC_GetPCLK1Freq()); printf("APB2 Timer Clock: %lu Hz\n", HAL_RCC_GetPCLK2Freq()); uint32_t apb1_prescaler = (RCC->D2CFGR & RCC_D2CFGR_D2PPRE1) >> RCC_D2CFGR_D2PPRE1_Pos; uint32_t apb2_prescaler = (RCC->D2CFGR & RCC_D2CFGR_D2PPRE2) >> RCC_D2CFGR_D2PPRE2_Pos; printf("APB1 Prescaler: %lu\n", apb1_prescaler); printf("APB2 Prescaler: %lu\n", apb2_prescaler); uint32_t pclk1 = HAL_RCC_GetPCLK1Freq(); // Get APB1 clock uint32_t pclk2 = HAL_RCC_GetPCLK2Freq(); // Get APB2 clock printf("APB1 Clock: %lu Hz\n", pclk1); printf("APB2 Clock: %lu Hz\n", pclk2); // If prescaler > 1, Timer Clock = PCLK * 2 if (apb1_prescaler > 3) { // Values >3 mean prescaler is applied printf("APB1 Timer Clock: %lu Hz\n", pclk1 * 2); } else { printf("APB1 Timer Clock: %lu Hz\n", pclk1); } if (apb2_prescaler > 3) { printf("APB2 Timer Clock: %lu Hz\n", pclk2 * 2); } else { printf("APB2 Timer Clock: %lu Hz\n", pclk2); }
View more
 
Does anyone have any suggestion what I am doing wrong?

Edited Code Format 




7 REPLIES 7
Sarra.S
ST Employee

Hello @PetrK

Given that the discrepancy is huge, in the order of 50MHz for APB1 and APB2, i suspect there is maybe an issue with the measurement method! 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @Sarra.S ,

thank you for the reply, I think that it is not measurement method - also have to set the timers regarding to the value ato be able run the servos. The real frequency is real.
I also have to add the 153.6 MHz into the SWV settings to get the printf values.  

PetrK_0-1744109072196.png

Should it be some power issue? I am powering the Nucleo

through USB from notebook.

MasterT
Lead

In case of ambiguity, use hardware - oscilloscope verification driving MCO1 / MCO2 outputs, there 5 /6 control check points for each

Sarra.S
ST Employee

Hello @PetrK, any updates on this matter? 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

PetrK
Associate II

Hello,
I goes through the user manual once again and realize that the inputed HSE frequency is provided by ST LINK MCO - 8 Mhz. There was set authomaticly 25 Mhz in the clock configuration. 

https://www.st.com/resource/en/user_manual/um2408-stm32h7-nucleo144-boards-mb1363-stmicroelectronics.pdf
7.9.1

I followed tutorial paths for set HSE, but nobody mentioned, that it is necessary to improve the solder bridges on the board to connect the external oscillator. This is my first STM32 board, so I do not know if it is standard or something special for my H7 version.

 


.  

Hello,

Indeed by default the HSE clock source is generated by the STLINK MCO:

mALLEm_0-1744627580541.png

From the board schematics, SB72 is soldered by default:

mALLEm_0-1744628900273.png

And the HSE crystal is not available (DNF: Do Not Fit):

mALLEm_1-1744627839326.png

See also this article: How to use STLINK-V3 MCO output on Nucleo boards as a precise clock source for STM32

In any case, anyone needs to start with a ST board he needs first to download the board documentation especially the User manual and the schematic.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

" I followed tutorial paths for set HSE, but nobody mentioned, that it is necessary to improve the solder bridges on the board to connect the external oscillator. This is my first STM32 board, so I do not know if it is standard or something special for my H7 version. "

What kind of tutorial ?

Nucleo working as it is, AFAIK ST-Link always provides clock on any nucleo boards, with option 8 or 8.33 MHz.

No hardware re-config required. Simply enter 8 MHz into box instead of 25.  Likely software StmCubeMX bug or you start project in another way - from uCPU selector instead of board selector.