2025-06-12 6:28 AM
Why I do not find the receiver frequency setting in the LPAWUR_WakeupRadio_Rx code?
While I can find the transmitter frequency setting in MRSUBG_WakeupRadio_Tx
as MRSUBG_RadioInitStruct.lFrequencyBase = 868000000;
2025-08-01 2:52 AM
Hello @Gwo
The LPAWUR is listening to all wake-up signal from all the frequency band covered by this peripheral. So, the frequency is not set by SW but it is limited by the frequency band of the LPAWUR and the HW supported frequency.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.