cancel
Showing results for 
Search instead for 
Did you mean: 

Why sample projects do not include a .ioc file ?

yilmazkircicek
Associate III

Hi All,

Is there anyone knows why sample projects do not include a .ioc file ?

Are not these project generated with CubeMx ?

https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects

 

Regards.

 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

They're not made using STM32CubeMX.

You can translate them yourself with some effort.

Creating a STM32CubMX ioc project for older STM32C... - STMicroelectronics Community

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

4 REPLIES 4
TDK
Super User

They're not made using STM32CubeMX.

You can translate them yourself with some effort.

Creating a STM32CubMX ioc project for older STM32C... - STMicroelectronics Community

If you feel a post has answered your question, please click "Accept as Solution".
TDK
Super User

There are some benefits to not providing IOC files. The Cube software is constantly being updated. Despite the best intentions, sometimes bugs are introduced, sometimes IOC files may not be 100% compatible. Providing IOC files would increase the burden here.

A modestly skilled programmer should be able to get up and running provided the examples. The "Example Selector" in STM32CubeMX facilitates this even more.

It doesn't seem unreasonable to me.

If you feel a post has answered your question, please click "Accept as Solution".
Andrew Neil
Super User

@yilmazkircicek wrote:

Is there anyone knows why sample projects do not include a .ioc file ?


Some do; some don't:

https://community.st.com/t5/stm32-mcus-products/some-example-projects-don-t-use-ioc-file/m-p/698338/highlight/true#M255312

 

Possible way to tell which is which:

https://community.st.com/t5/stm32-mcus-products/some-example-projects-don-t-use-ioc-file/m-p/698408/highlight/true#M255333

 


@yilmazkircicek wrote:

Are not these project generated with CubeMx ?


Presumably not.

 


@yilmazkircicek wrote:

it does not seem reasonable for a customer viewpoint


Not all customers will use CubeMX anyhow - so, I guess, it's reasonable to have some examples which demonstrate the alternative.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@Andrew Neil wrote:

@yilmazkircicek wrote:

Is there anyone knows why sample projects do not include a .ioc file ?


Some do; some don't:


And the ones which don't usually have a Board Support Package (BSP) to abstract the hardware details and, thus, facilitate the manual re-configuration...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.