2016-12-08 1:32 PM
Hi,
I am trying to build something and currently doing some evaluation and development with 32L476GDISCOVERY Discovery Kit with STM32L476VG microcontroller.
What I am trying to achieve at the moment is output of integrated MEMS microphone into a buffer via DMA.
Everything seems to be working perfectly except for one, for me quite important, thing - the resolution of the samples is much higher then I expect. But I need the target buffer to be array of half words (16bits).
Setup I am trying:
DFSDM input clock frequency: 24MHz
Output clock divider: 8 (it means 24/8 = 3Mhz for MEMS microphone)
Filter is using regular conversion
Filter order: 2 (Sinc2)
Continuous mode: ENABLED
DMA Mode: ENABLED
Filter oversampling (Fosr): 73 (=> output sample rate = 3MHz/73 = 41095Hz - almost 41.1kHz)
Integrator oversampling (Iosr): 1
According to
, where table 124 on page 621 (chapter 21.2.8 Digital filter configuration) defines how to compute maximum output resolution, I should be getting something between +/- 73^2 = +/- 5329. But I am getting much higher numbers.Small example of data I am getting: 19200, 16640, 17152, 14080, 14592, 12544, 10496, 11008, 7424, 6400, 6912, 4864,2304, 2304, -256, 768, -768, -2816, -2304, -3328, -1792
They are obviously bigger than +/-5329.
Does somebody have any idea why it could be happening?
I know I can for example use bit shift to align it to size I require, but since it does not behave as expected, I am afraid I am doing something completely wrong. If I decide to use bit shift I am also not sure what number I should use, since I do not know what can be the peak value of my filter output at the moment.
My filter and channel initialization procedure:
hdfsdm1_filter1
.
Instance=
DFSDM1_Filter1;
hdfsdm1_filter1.
Init.
RegularParam.
Trigger=
DFSDM_FILTER_SW_TRIGGER;
hdfsdm1_filter1.
Init.
RegularParam.
FastMode=
ENABLE;
hdfsdm1_filter1.
Init.
RegularParam.
DmaMode=
ENABLE;
hdfsdm1_filter1.
Init.
FilterParam.
SincOrder=
DFSDM_FILTER_SINC2_ORDER;
hdfsdm1_filter1.
Init.
FilterParam.
Oversampling=
73
;
hdfsdm1_filter1.
Init
.
FilterParam
.
IntOversampling
=
1
;
hdfsdm1_channel2.
Instance
=
DFSDM1_Channel2
;
hdfsdm1_channel2.
Init
.
OutputClock
.
Activation
=
ENABLE
;
hdfsdm1_channel2.
Init
.
OutputClock
.
Selection
=
DFSDM_CHANNEL_OUTPUT_CLOCK_SYSTEM
;
hdfsdm1_channel2.
Init
.
OutputClock
.
Divider
=
8
;
hdfsdm1_channel2.
Init
.
Input
.
Multiplexer
=
DFSDM_CHANNEL_EXTERNAL_INPUTS
;
hdfsdm1_channel2.
Init
.
Input
.
DataPacking
=
DFSDM_CHANNEL_STANDARD_MODE
;
hdfsdm1_channel2.
Init
.
Input
.
Pins
=
DFSDM_CHANNEL_SAME_CHANNEL_PINS
;
hdfsdm1_channel2.
Init
.
SerialInterface
.
Type
=
DFSDM_CHANNEL_SPI_RISING
;
hdfsdm1_channel2.
Init
.
SerialInterface
.
SpiClock
=
DFSDM_CHANNEL_SPI_CLOCK_INTERNAL
;
hdfsdm1_channel2.
Init
.
Awd
.
FilterOrder
=
DFSDM_CHANNEL_FASTSINC_ORDER
;
hdfsdm1_channel2.
Init
.
Awd
.
Oversampling
=
1
;
hdfsdm1_channel2.
Init
.
Offset
=
0
;
hdfsdm1_channel2.
Init
.
RightBitShift
=
0x00
;
?
?
?
?
?
?
?
?
?
?
?
?
?
?
?
?
?
?
?
?
?
?
Thank you for your advice
Roman
#stm32l476 #mems #discovery #problem #filter #dfsdm2016-12-09 7:44 AM
Hi
bosakrom
,ST is providing an example about theDFSDM usage. This will surely help you to correctly configure yourperipheral.
You can find the working 'DFSDM_AudioRecord' example
inside the STM32Cube
L
4 library (v 1.6.0)
at this path:STM32Cube_FW_L4_V1.6.0\Projects\STM32L476G-Discovery\Examples\DFSDM\DFSDM_AudioRecord.
May this help you.
Best regards,
Lawliet
If this answers your request, please press 'correct'
:)
2016-12-10 3:10 PM
Hi
garsi.khouloud
,thank you very much for the quick reply.
I know about the example and tried it already before. After you mentioned it I tried it again with focus on getting same data I have for my case and it seems there is same problem. I tried to debug it and after I paused I checked RecBuff data.
According to DFSDM setup of the example:
Filter order: 3(Sinc3)
Continuous mode: ENABLED
DMA Mode: ENABLED
Filter oversampling (Fosr): 64
Integrator oversampling (Iosr): 1
Right bit shift: 2
I would expect to get resolution +/-65536 = 64^3 >> 2 (based on equations and other definitions from reference manual mentioned above)
But I again get quite different numbers.
Example data from RecBuffer:-840192,-709888,-585728,-460288,-315904,-174080,-24064,106752,237056,385536,506880,621824
As you can see, majority of the values are much higher thanexpected maximum again.
Do I overlook something? Any more ideas?
Thank you
Roman