Posted on December 14, 2016 at 19:42Hi reh.tilmann,If you want to use the PB3 as a GPIO pin, you should not use the asynchronous trace over the SW debug.Lawliet.
Posted on December 14, 2016 at 18:09Hi,In 'STM32F1 getting started hardware development' application note , you can see that PB3 is used by the SW debug port. PB5 and PA15 are only used by JTAG, this is why you can use them as GPIO pins by disabling...
Posted on December 14, 2016 at 16:04Hi Hans,Are you measuring the interrupt response time on the first iteration? Could you give as the response times for the second and the third iterations?If you will use the STM32F7, I advise you to use the ITCM ...
Posted on December 14, 2016 at 14:12 Hi Grodetsky.Yury , I advise you to use SW4STM32 IDE. It gives you the ability to create your own custom board. Regards, Lawliet.
Posted on December 13, 2016 at 15:55Hi Paul,Do not forget to connect the new VDD/VDDIO2/VSS pins.And, your migtation to STM32F091 should be fine.Regards,Lawliet.