2023-10-03 1:48 AM
I want to design an Intuitive System with a 1280x 800 LCD interface with RGB 888 running Fluidic Animations and transitions (30FPS) Which system combination will work to create such a system? I figured it would require STM32H750 Or similar MCu with 32 BIT RAM Interface 24 Bits RGB Along with QUAD FLASH.
Solved! Go to Solution.
2023-10-26 9:27 AM - edited 2023-10-26 9:31 AM
calculated values dot clock is in table... from this number FPS= DCLK / (1280x800) for example 16bitram 24bit dma2d FPS = 38000000/1024000 = 37FPS
2023-10-04 8:43 AM
Waiting for inputs...
2023-10-04 9:11 AM
I create 1280x480 DSI RGB565 on F469. Your idea is on edge for internal MCU bus capacity. You can try F7xx or H7xx Read apnote about LTDC LCD-TFT display controller (LTDC) on STM32 MCUs - Application note
2023-10-04 10:46 AM - edited 2023-10-14 1:49 AM
Thanks for the input.
2023-10-14 1:47 AM
Waiting for feedback.
2023-10-14 1:50 AM
I have gone through the App note and I am some what stuck at 1280x800 Resolution at RGB 888 With 24bit Color Depth if I am running the CPU with 32 Bit RAM.
How much FPS Would I get If I am running the System with IS42S32400F-6BL in 32BIT mode
2023-10-15 1:04 PM
Any Update?
2023-10-25 2:03 AM
@jiangfanPlease provide your feedback on this.
2023-10-25 2:29 AM
I think Mohammad MORADI has more expertise on this topic. You may try to ask Mohammad.
2023-10-25 3:02 AM
@Mohammad MORADI ESFAHANIASLPlease loop in.