cancel
Showing results for 
Search instead for 
Did you mean: 

Designing a Intuitive System with 1280x 800 LCD Interfaced with RGB 888 with Fluidic Animations

ZExpo.1
Senior

I want to design an Intuitive System with a 1280x 800 LCD interface with RGB 888 running Fluidic Animations and transitions (30FPS) Which system combination will work to create such a system? I figured it would require STM32H750 Or similar MCu with 32 BIT RAM Interface 24 Bits RGB Along with QUAD FLASH.

1 ACCEPTED SOLUTION

Accepted Solutions

MM1_0-1698337594494.png

calculated values dot clock is in table... from this number FPS= DCLK / (1280x800) for example 16bitram 24bit dma2d FPS = 38000000/1024000 = 37FPS

View solution in original post

16 REPLIES 16
ZExpo.1
Senior

Waiting for inputs...

MM..1
Chief III

I create 1280x480 DSI RGB565 on F469. Your idea is on edge for internal MCU bus capacity. You can try F7xx or H7xx  Read apnote about LTDC LCD-TFT display controller (LTDC) on STM32 MCUs - Application note

Thanks for the input.

ZExpo.1
Senior

Waiting for feedback.

ZExpo.1
Senior

I have gone through the App note and I am some what stuck at 1280x800 Resolution at RGB 888 With 24bit Color Depth if I am running the CPU with 32 Bit RAM.
How much FPS Would I get If I am running the System with IS42S32400F-6BL in 32BIT mode

ZExpo.1
Senior

Any Update?

ZExpo.1
Senior
 

@jiangfanPlease provide your feedback on this.

I think Mohammad MORADI has more expertise on this topic. You may try to ask Mohammad.