2020-11-13 06:31 AM
Dear Sir,
Debug and driver folders are not created in code generation
Debug option is also not highlighted in menu button.
Below is the screenshot of that
please help.
2020-11-19 05:41 AM
Hello @Byede.1 ,
Please provide a log file that will help our CubeMX team to analyse the issue.
Imen
2020-11-19 07:04 PM
2020-11-19 09:49 PM
2020-11-20 12:43 AM
Hi @Byede.1 ,
Can you please share the ioc file, as well the log file that can be found in your user directory under the .stm32cubemx folder.
Imen
2020-11-20 03:23 AM
2020-11-20 03:24 AM
2020-11-23 06:08 AM
Hello @Byede.1
Tested the same scenario without getting issue.
I would like to know if you use a proxy or not because; if you don't use a proxy, with Direct and Native, you don't have to fill in the fields (you have to leave them all empty), on the other hand if you use a proxy, you have to fill in HTTP and HTTPS.
Best regards,
Nesrine
2020-11-23 06:31 AM
2020-11-23 06:38 AM
Hello @Byede.1
Go to window ==> preference
Best regards,
Nesrine