cancel
Showing results for 
Search instead for 
Did you mean: 

Debug and driver folders are not created in code generation

Byede.1
Associate II

Dear Sir,

 Debug and driver folders are not created in code generation

Debug option is also not highlighted in menu button.

Below is the screenshot of that

0693W000005BK6VQAW.png 

please help.

11 REPLIES 11
Dear San,
Iam completely new to STM32 CubeIDE.
Here is the screenshot of windows==> Preferences.
[image: image.png]
Tell me what i can set.
*Thanks & RegardsY. Bala Nagendra *

Hi @Byede.1​ 

If you are using Proxy, you should go to windows==> Preferences ==> Network Connections then you have to fill in HTTP and HTTPS (Host and port).

If you don't use a Proxy, with Direct and Native "Active Provider", you don't have to fill in the fields (you have to leave them all empty).

Best regards,

Nesrine