cancel
Showing results for 
Search instead for 
Did you mean: 

How does the USART 2 transmit signal output from pins PA2 and GND to a logic analyser?

SWall.2
Associate II

I am having a little difficulty getting a USART 2 signal to output to a logic analyser using transmit Tx serial asynchronous communication. I have configured a USART 2 peripheral to communicate through a DMA. The GPIO pin PA2 is outputting a constant logic one, so I am guessing I have missed something on the STML476VG DISCO microcontroller. I have tried to set the LSE clock to 32.768 kHz to no success. I have the low power sleep mode HAL driver configured in the source code. I have tried to change the parity setting in the IDE to even, but no luck.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

UART sends signals with a pattern of 0s and 1s. If you're not seeing any change in the level, it's not sending info (or you're not capturing it correctly).

Get it working in blocking mode first (HAL_UART_Transmit) then move up to DMA after that (HAL_UART_Transmit_DMA).

If you feel a post has answered your question, please click "Accept as Solution".
SWall.2
Associate II

Thanks for getting back to me.I'll give the UART peripheral a go without the DMA and see if I can get a signal to transmit.Thanks again.