2017-07-18 7:34 AM
Hello,
I'm new to CubeMX and HAL drivers. Recently I build a test project with RTC module, but now I'm experiencing quite weird behavior of the HAL_RTC_GetTime/HAL_RTC_GetDate.
In my case HAL_RTC_GetTime function can return Hours values which is greater then 24 .... and Date is also not incrementing ...
I have standard initialization code from STM32CubeMX (updated today, no change).
Thanks
#rtc-hal #stm32f4072017-07-18 8:12 AM
You see 24 hours after having rolled over from 23 hours?
There is no magic in the RTC, if you set it to garbage e.g. 24 hours it will run up to 32 and then rolls over to 0.
JW
2017-07-18 11:31 AM
No I did set it to 23:59:00, and after a minute the time showed me 24:00 ..........
2017-07-18 11:33 AM
You say 32 haha , I leave it running and now it showing 2017-07-17 35:02:30 ... what am I doing wrong ?!
2017-07-18 12:58 PM
Ah, it's BCD, so up to 39 hours.
what am I doing wrong?
My guess is that you have RTC_CR.FMT set to AM/PM.
JW
2017-07-19 12:46 AM
weird, here is the code samples from the initialization and the way how I'm getting date and time:
/* RTC init function */
void MX_RTC_Init(void)
{
RTC_TimeTypeDef sTime;
RTC_DateTypeDef sDate;
/**Initialize RTC Only
*/
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = 127;
hrtc.Init.SynchPrediv = 255;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Initialize RTC and set the Time and Date
*/
if(HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR0) != 0x32F2){
sTime.Hours = 0;
sTime.Minutes = 0;
sTime.Seconds = 0;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_SET;
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BIN) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
sDate.WeekDay = RTC_WEEKDAY_TUESDAY;
sDate.Month = RTC_MONTH_JULY;
sDate.Date = 9;
sDate.Year = 17;
if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BIN) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
HAL_RTCEx_BKUPWrite(&hrtc,RTC_BKP_DR0,0x32F2);
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
And here is how i getting date and time:
RTC_TimeTypeDef time;
RTC_DateTypeDef date;
if(HAL_RTC_GetTime( &hrtc, &time, RTC_FORMAT_BIN ) != HAL_OK){
dev_sprintf(io->stream,'
Error getting time
');
return 0;
}
if(HAL_RTC_GetDate( &hrtc, &date, RTC_FORMAT_BIN ) !=HAL_OK){
dev_sprintf(io->stream,'
Error getting time
');
return 0;
}
dev_sprintf(io->stream,'Current date: %04d-%02d-%02d %02d:%02d:%02d
',
date.Year+CFG_DATE_MILLENNIUM,
date.Month +1, // 0..11
date.Date +1, // 0..30
time.Hours,
time.Minutes,
time.Seconds);�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
If this is a BCD format, then tell me, how can I get a Binary date from HAL driver ?
Thanks
2017-07-19 1:36 AM
hello!
I faced recently this kind of problem and i solved it. (it was because time structure was not corectly initialised)
First of all check (in case you have ) the voltage of VBAT.
Make a backup domain reset.
Set the Clock and Date (it is important to set them both)
dont forget to correctly and fully initialize the time and date structures.
an example is :
RTC_DateTypeDef dt;
RTC_TimeTypeDef tt; tt.Hours=xxx; tt.Minutes=xxx; tt.Seconds=xxx; tt.SecondFraction=0; tt.SubSeconds=0; tt.DayLightSaving=xxx; tt.TimeFormat=RTC_HOURFORMAT12_AM;// tt.StoreOperation=RTC_STOREOPERATION_RESET; dt.Date=xxx; dt.Month=xxx; dt.Year=xxx; dt.WeekDay=xxx;hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = 127;// I use 32768 crystal hrtc.Init.SynchPrediv = 255;hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;HAL_RTC_Init(&hrtc); HAL_RTC_SetTime(&hrtc, &tt, RTC_FORMAT_BIN);// or bcd ofcourseHAL_RTC_SetDate(&hrtc,&dt, RTC_FORMAT_BIN);// or bcd ofcourseCheck the input values xxx to be inside the limits.
finaly when you decide to read clock read both time and date.
2017-07-19 2:58 AM
Put a new limit for hours
Current date: 2017-07-17 39:18:25
2017-07-19 12:24 PM
Thank you so much, that does solved not all but part of the issues.
Now time structure looks like working OK, but date doing same weird increments. But now I know where to dig in ...
Thanks !