2024-12-30 9:51 PM - edited 2024-12-30 9:57 PM
Hey,
I am using one of the custom board for stm32f407vetx. When i was using stm32f407 disc board. There was no problem but now i cannot fill up array with float or double values. And yes i increase min heap size to 0x1000 and max heap size to 0x2000. Also i check the box which is "-u_printf_float". Is there any any help?
Thanks.
Edit: i realize i open the topic wrong side of the forum. Sorry for that.
Solved! Go to Solution.
2024-12-30 11:28 PM
I solved this issue. When i first time debug project i didn't check the "-u_printf_float" box. When i delete debug files and redebug it, its been solved.
2024-12-30 11:28 PM
I solved this issue. When i first time debug project i didn't check the "-u_printf_float" box. When i delete debug files and redebug it, its been solved.