cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX on Linux fails to generate FSMC MSP code

frackers
Senior
Posted on October 24, 2017 at 04:11

Running latest 4.1 STM32CubeMx on both *buntu and Windows 7 and the generated stm32f4xx_hal_msp.c is totally different. The HAL libraries in both cases areSTM32Cube_FW_F4_V1.0.

With the Linux version, the following functions are missing:

  • HAL_FSMC_MspInit
  • HAL_SRAM_MspInit
  • HAL_FSMC_MspDeInit
  • HAL_SRAM_MspDeInit

which results (not surprisingly) a totally useless build.

This needs to be fixed urgently as I only have part-time access to a single windows machine to create the code if I change any pinouts etc.

Note: this post was migrated and contained many threaded conversations, some content may be missing.
This discussion is locked. Please start a new topic to ask your question.
25 REPLIES 25
Posted on March 16, 2018 at 16:09

I'm toying with the idea of making my own CubeMX for the Nucleo I have...

I'm oscillating between Processing (a fast mode in getting a nice graphical interface which I need for the clock setup), Lazarus+FreePascal (easy file manipulation, easy string manipulation and RAD) and Qt with C++...

It will generate for Makefile projects with LL drivers. Another option (and a strong temptation) is to make it generate for SPL.

frackers
Senior
Posted on April 04, 2018 at 03:27

Over 5 months in and still not even an acknowledgement of the problem.

Does anyone know of a way of escalating the issue with ST to at least get some confirmation that I'm not the only one with this issue?

This continues to impact my development and will now start to influence my choices of WIFI, BlueTooth, Accelerometer and NFC devices (currently 

SPWF01, SPBTLE-RF, LSM6DSL, 

CR95HF)  if I can't get reliable product support.

Imen.D
ST Employee
Posted on April 04, 2018 at 12:30

Hello,

I will raise you request to the appropriate team for investigation.

Sorry for the inconvenience it may bring.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on April 25, 2018 at 13:51

Hi Frackers,

Thanks for your feedback and s

orry for late response.

I confirm the bug. The issue will be fixed in the next CubeMX release.

Please feel free to contact me for further details.

Best regards,

Mohamed

Posted on May 14, 2018 at 06:21

Just updated to 4.25.1 and it STILL doesn't work.

Posted on May 14, 2018 at 11:31

Hi

Gilks.Robin

,

This issue will be fixed for the next release CubeMX 4.26 .Sorry for such inconvenience.

Best regards,

Mohamed.