Stacking IHM06A1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-14 2:29 AM
Posted on May 14, 2018 at 11:29
I'm hoping someone can provide a straight-forward answer as to how I can operate multiple stepper motors using stacked IHM06A1 boards. In example code, the STSpin220 class is initialised as
motor = new STSpin220(D2, D8, D7, D5, D10, D3, PWM_REF_PIN);
Is there a simple way of declaring two 'motors' in this way, perhaps with a small hardware mod?
Thanks
#stepper-motor #stspin220 #ihm06a1
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0