Question
CubeMX on Linux fails to generate FSMC MSP code
Posted on October 24, 2017 at 04:11
Running latest 4.1 STM32CubeMx on both *buntu and Windows 7 and the generated stm32f4xx_hal_msp.c is totally different. The HAL libraries in both cases areSTM32Cube_FW_F4_V1.0.
With the Linux version, the following functions are missing:
- HAL_FSMC_MspInit
- HAL_SRAM_MspInit
- HAL_FSMC_MspDeInit
- HAL_SRAM_MspDeInit
which results (not surprisingly) a totally useless build.
This needs to be fixed urgently as I only have part-time access to a single windows machine to create the code if I change any pinouts etc.
Note: this post was migrated and contained many threaded conversations, some content may be missing.