cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMx missing I2C2 STM32F051C6Tx

Sebastian Juch
Associate II
Posted on August 27, 2015 at 09:50

Hi , i'm currently developing a circuit with the STM32F051C6Tx.

When i select the Cpu in CubeMx i can not selct the I2C2 on PB10/PB11, there is just the I2C1 on PB7/PB6. As i read in the Datasheet befor there have to be a I2C2 on PB10/11 (Datasheet Page33/115). So the question, is the Datasheet wrong or is the I2C2 simple missing in CubeMx ?

Regards, Sebastian
2 REPLIES 2
Posted on August 27, 2015 at 11:54

Hi Sebastian J.,

Go to the page 10/115 (table2), the third footnote indicates that I2C2 is not present. So, ther is no bug related to CubeMx.

-Shahrzad-

Sebastian Juch
Associate II
Posted on August 27, 2015 at 12:29

Your right. Thank you . It was my fault. So i have to use I2C1.

Regards, Sebastian