2015-08-27 12:50 AM
Hi , i'm currently developing a circuit with the STM32F051C6Tx.
When i select the Cpu in CubeMx i can not selct the I2C2 on PB10/PB11, there is just the I2C1 on PB7/PB6. As i read in the Datasheet befor there have to be a I2C2 on PB10/11 (Datasheet Page33/115). So the question, is the Datasheet wrong or is the I2C2 simple missing in CubeMx ? Regards, Sebastian2015-08-27 2:54 AM
Hi Sebastian J.,
Go to the page 10/115 (table2), the third footnote indicates that I2C2 is not present. So, ther is no bug related to CubeMx. -Shahrzad-2015-08-27 3:29 AM
Your right. Thank you . It was my fault. So i have to use I2C1.
Regards, Sebastian