2018-08-16 01:26 AM
Hi, since update to cubeMx Version 4.26.1 filenames for .project and .cproject disapear in the project folder. Does anyone have clue what the reason could be? Is there a possibility to downgrade Cuibe MX? Could it be a win10 issue? Thats something new....
Even Projects i did not open in cubemx are gone, which means it could be a win 10 issue
Attached you find a screenshot
2018-08-16 03:08 AM
Dear @Community member ,
I Have generated a project using STM32CubeMX 4.26.1 and I'm not facing the issue you're highlighting on windows7.
Below is a screenshot of the generated files:
Khouloud.
2018-08-20 06:43 AM
well maybe its a windows bug. I will live with it since i dont have time to spend on this.
Thanks