cancel
Showing results for 
Search instead for 
Did you mean: 

Regarding Boot loader

Manoj Hiwarkar
Associate III

Hello,

Sir I want know that whether the boot loader code is already present in the STM32 MCUs by default ? or we have to download it.

Regards,

Manoj Hiwarkar

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6

It is in OTP/ROM at delivery

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
RN
Senior

Hello Manoj,

Bootloader is in the system memory of MCU. by default MCU doesnot execute it. you have to configure the boot pins given.

check here : https://www.st.com/content/ccc/resource/technical/document/application_note/b9/9b/16/3a/12/1e/40/0c/CD00167594.pdf/files/CD00167594.pdf/jcr:content/translations/en.CD00167594.pdf

Manoj Hiwarkar
Associate III

thank you sir. Sir one more query i have can you please tell me howto send one string "HELLO". using  HAL_CAN_Transmit function i have searched a lot but couldn't get a satisfied answer.

That's not really how CAN functions. You have an 8-byte data payload, you'd need to place your ASCII data within that.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Manoj Hiwarkar
Associate III

sir can i get one example program of the same ? it will be a great help.

Look at the examples provided in the HAL/Cube trees for the unspecified STM32 part you are using.

...

       /* Set the data to be transmitted */

       TxData[0] = 'H';

       TxData[1] = 'E';

       TxData[2] = 'L';

       TxData[3] = 'L';

       TxData[4] = 'O';

TxHeader.DLC = 5; // Length

       /* Start the Transmission process */

       if (HAL_CAN_AddTxMessage(&CanHandle, &TxHeader, TxData, &TxMailbox) != HAL_OK)

       {

         /* Transmission request Error */

         Error_Handler();

       }

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..