cancel
Showing results for 
Search instead for 
Did you mean: 

CTSIZE becomes 0x01 after SPI communication is completed

pass3master
Associate III

Regarding the problem that CTSIZE becomes 0x01 after SPI communication is completed,

In our program, SPI-SR-CTSIZE becomes 0x01 after SPI communication is completed.
In that state, if we try to perform the next SPI communication, a timeout error occurs in the middle of the communication.
When SPI-SR-CTSIZE = 0, no timeout error occurs.
Is there any way to set SPI-SR-CTSIZE (= TSIZE number of frames in a session) to 0?

Translated with DeepL.com (free version)

0 REPLIES 0