Skip to main content
Associate II
October 31, 2024
Solved

Looking for Compact, Low-Power Alternative to STM32F401CCU6

  • October 31, 2024
  • 2 replies
  • 1402 views

Hello everyone,

I'm currently using the STM32F401CCU6 in my project, but it's proving to be oversized for my application, both in terms of physical package and power requirements. I'm hoping to switch to a smaller STM32 microcontroller that maintains as much compatibility as possible with the F4 series, so I can avoid major changes to my implementation.

Here are my main requirements:

12-Pin Package (a few more pins are okay, but aiming for a minimal footprint)

RTC Support with a 32.768 kHz external oscillator

SPI Communication capabilities

Low-Power Modes (ideally STOP, STANDBY, or similar ultra-low power options)

 

Any recommendations for STM32 microcontrollers that meet these criteria? I’d love to hear about your experiences with similar switches, too!

Thank you in advance!

 

2 replies

Andrew Neil
Andrew NeilBest answer
Super User
October 31, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
wardAuthor
Associate II
October 31, 2024

Thanks for the provided links.

ST Employee
October 31, 2024
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
wardAuthor
Associate II
October 31, 2024

Thank you for the suggestion. I’ll take it into consideration.