Creating a professional Firmware update scheme for STM32
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-03-12 10:41 AM - edited 2024-03-12 1:42 PM
I'm working with a commercial-grade food-service product that uses the STM32L073 in conjunction with an android tablet connected over UART or Bluetooth. For our next-gen product, we're investigating methods to economically implement firmware updates on a fleet of a few thousand units. The one major factor is that we have limited resources (one part-time firmware developer with no filesystem or bootloader experience, along with a part-time electrical engineer), so maximizing implementation speed is key. We have the following options we are exploring for firmware updates:
1. Currently the only method implemented to perform firmware updates is using a ST-Link Programmer. Our issues with this setup is that:
- requires the user open up the product
- requires the user plug the ST link onto the pcb (electrically risky)
- Requires a laptop
- ST-Link can be lost
- anyone can flash unofficial firmware
2. Switch to an STM32WB:
- Seems to require either a laptop or phone with the propriety ST app
- anyone can flash unofficial firmware
- Requires porting firmware/pcb to STM32WB
3. Switch to Golioth IoT Platform (replace the ST board)
- Requires porting code to new platform
- Requires fleet management
- Expensive
4. Flash Drive:
- Requires bootloader / file system implementation for which I've struggled to find examples. Presumably requires a significant amount of development time.
- anyone can flash unofficial firmware
5. SD card:
- Requires bootloader / file system implementation for which I've struggled to find examples.
- SD card readers are less common than usb ports.
- anyone can flash unofficial firmware
Which of these 4 options would you recommend committing to for this next generation product, and what resources can I refer to help understand the implementation? Thanks!
- Labels:
-
Flash
-
STM32L0 Series
-
USB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-03-15 6:19 AM - edited 2024-03-15 6:50 AM
@waclawek.jan That's the point. I believed too that sellers of such modules have all formalities settled, but, as always, better check this with a lawyer (( For food delivery it may pass easily.

- « Previous
-
- 1
- 2
- Next »