Creating a professional Firmware update scheme for STM32
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-12 10:41 AM - edited ‎2024-03-12 1:42 PM
I'm working with a commercial-grade food-service product that uses the STM32L073 in conjunction with an android tablet connected over UART or Bluetooth. For our next-gen product, we're investigating methods to economically implement firmware updates on a fleet of a few thousand units. The one major factor is that we have limited resources (one part-time firmware developer with no filesystem or bootloader experience, along with a part-time electrical engineer), so maximizing implementation speed is key. We have the following options we are exploring for firmware updates:
1. Currently the only method implemented to perform firmware updates is using a ST-Link Programmer. Our issues with this setup is that:
- requires the user open up the product
- requires the user plug the ST link onto the pcb (electrically risky)
- Requires a laptop
- ST-Link can be lost
- anyone can flash unofficial firmware
2. Switch to an STM32WB:
- Seems to require either a laptop or phone with the propriety ST app
- anyone can flash unofficial firmware
- Requires porting firmware/pcb to STM32WB
3. Switch to Golioth IoT Platform (replace the ST board)
- Requires porting code to new platform
- Requires fleet management
- Expensive
4. Flash Drive:
- Requires bootloader / file system implementation for which I've struggled to find examples. Presumably requires a significant amount of development time.
- anyone can flash unofficial firmware
5. SD card:
- Requires bootloader / file system implementation for which I've struggled to find examples.
- SD card readers are less common than usb ports.
- anyone can flash unofficial firmware
Which of these 4 options would you recommend committing to for this next generation product, and what resources can I refer to help understand the implementation? Thanks!
- Labels:
-
Flash
-
STM32L0 Series
-
USB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-12 10:52 AM - edited ‎2024-03-12 10:53 AM
> we have limited resources (one part-time firmware developer with no filesystem or bootloader experience, along with a part-time electrical engineer)
You can try to find help for your project here.
Also, instead of owning a laptop and other equipment, you can rent it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-12 11:12 AM
Surely a boot loader written with some thought can authenticate the firmware image so random/unofficial firmware don't get loaded. There's a) encryption, and b) public/private elliptical curve signing methods that will fit in STM32
Not sure of the SDIO and USB-HOST type support in L07x parts.
Delivery via chip/dongle that plugs in the device is something that's viable. Cheap/simple stand-alone flasher.
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
‎2024-03-12 12:55 PM
Simple micro-SD adapter with UART interface, a.k.a "Openlog Serial Data Logger".
STM32 can use this to read files from a SD card. The UART connector has to be designed. It is slow (~ 115200) but dirt cheap and easy to program.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-12 1:48 PM
The OpenLager uses an STM32F411 (512KB Flash)
https://store.myairbot.com/openlager.html
https://newbeedrone.com/products/newbeedrone-f411-openlager
https://github.com/d-ronin/openlager
For pushing updates via AN3155 (STM32 UART Protocol Loader) one can take a look at the update mechanism in the Arduino MKR WAN1300 github repo
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
‎2024-03-12 2:04 PM - edited ‎2024-03-12 2:05 PM
The OpenLager firmware on github looks like only logger.
Many openloggers sold on ebay have the sparkfun firmware, it can read existing files from SD and has many interesting options.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-12 3:47 PM
Well the d-Ronin guys haven't touched it in 8 years, but the hardware can be disabused to other applications, and the firmware for them delivered as a .BIN.
Yeah the software's not feature rich, but it's designed for very high speed data streams and uses 4-bit SDIO w/DMA
GHI Electronics had some ALFAT related products. https://docs.ghielectronics.com/hardware/filesystem/intro.html
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
‎2024-03-14 7:54 AM
> STM32L073 in conjunction with an android tablet connected over UART or Bluetooth
So, can't the update be delivered from that tablet via the UART connection? Isn't the Bluetooth just a BT-to-UART module connected to STM32 via UART too?
If both answers are yes, then on STM32 side it's the same problem set as with any UART-based bootloader, and we can then discuss them as such; and then you would also need to provide the software counterpart on the tablet side.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-14 5:13 PM
Bluetooth UART (HC-05 or newer BLE BM-70) is a viable idea. But wireless may need extra certification effort and security considerations.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-15 2:12 AM
As I understand it, it's already part of the product (although I don't know in what way exactly).
JW