Counter Problem in Timer Interrupt
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-07 11:42 AM
Hello,
I set a timer timer in global interrupt mode. I monitored successfully a GPIO toggling with desired interrupt frequency. But a counter didn't increase in every timer interrupt cycle it was stuck at 1. Do you have any suggestions about the problem?
Thank you,
if (timer_flag){
txConvertData = ReadCommandMask | (255 << 8);
HAL_GPIO_WritePin(IN_SPI2_CS_GPIO_Port, IN_SPI2_CS_Pin, GPIO_PIN_RESET);
hal_status = HAL_SPI_TransmitReceive(&hspi2, (uint8_t*) &txInConvertData, (uint8_t*) &rxInConvertData[j], 1, 100);
HAL_GPIO_WritePin(IN_SPI2_CS_GPIO_Port, IN_SPI2_CS_Pin, GPIO_PIN_SET);
HAL_Delay(100);
if (hal_status != HAL_OK) {
printf("HAL SPI TransmitReceive error: %d\r\n", (int) hal_status);
}
j = j + 1;
//timer_flag = 0;
}
if (j == 20000){
HAL_TIM_Base_Stop_IT(&htim10);
j = 0;
timer_flag = 0;
}
/* USER CODE BEGIN 4 */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim){
if (htim == &htim10){
timer_flag = 1;
HAL_GPIO_TogglePin(EV_CH1_GPIO_Port, EV_CH1_Pin);
}
}
/* USER CODE END 4 */
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-07 1:03 PM
What exactly do you mean by "But a counter didn't increase in every timer interrupt cycle it was stuck at 1"? What counter? The timer's CNT register? Your main code "j" variable?
If you are trying to read the CNT register inside the callback function, I would EXPECT it to be something like "1" every time. I presume the timer is set to interrupt on update (i.e. CNT == ARR), which means the CNT resets to zero and starts counting again. And by the time the HAL code calls your callback, it has incremented to 1.
BTW - make sure you have "timer_flag" declared as "volatile".
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-07 1:07 PM - edited ‎2023-11-20 8:45 AM
I mean j variable.
The current setting of the timer is like that,
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-07 3:10 PM
That's probably because of HAL_Delay() call blocking the dtetection of flag set by timer interrupt.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-07 5:43 PM
@AE104​ ,
From what I see that is possibly the problem that you're facing is the timer_flag variable. Even though in HAL_TIM_PeriodElapsedCallback interrupt you are setting timer_flag = 1, in you main loop your if(timer_flag) will be false, so it won't run that part of the code to increment j variable.
So just like @Bob S​ said, be sure to have timer_flag declared as volatile so it isn't optimized, like...
volatile uint32_t timer_flag = 0;
Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!
If you find my solution useful, please click the Accept as Solution so others see the solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-10 8:03 AM
Right, the j value is not increasing even I set the timer_flag as volatile.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-10 8:19 AM
Post the function that the if statement is in. I suspect the variable j is declared local
Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!
If you find my solution useful, please click the Accept as Solution so others see the solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-10 8:37 AM
Sure.. Yes the j is local.
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_ADC1_Init();
MX_DAC_Init();
MX_SPI2_Init();
MX_SPI3_Init();
MX_USART2_UART_Init();
MX_USART3_UART_Init();
MX_I2C2_Init();
MX_TIM10_Init();
MX_TIM11_Init();
MX_TIM13_Init();
MX_TIM14_Init();
MX_TIM1_Init();
/* USER CODE BEGIN 2 */
HAL_TIM_Base_Start(&htim10); //initializes Timer 10
HAL_TIM_Base_Start_IT(&htim10); //initializes Timer 10
HAL_StatusTypeDef hal_status;
uint16_t j = 0;
uint16_t rxInCalibrateData[30];
uint16_t txInCalibrateData[30];
uint16_t txInConvertData;
uint16_t rxInConvertData[20002];
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
for (int i = 0; i < 30; i++) {
HAL_GPIO_WritePin(IN_SPI2_CS_GPIO_Port, IN_SPI2_CS_Pin, GPIO_PIN_RESET);
hal_status = HAL_SPI_TransmitReceive(&hspi2, (uint8_t*) &txInCalibrateData[i], (uint8_t*) &rxInCalibrateData[i], 1, 100);
HAL_GPIO_WritePin(IN_SPI2_CS_GPIO_Port, IN_SPI2_CS_Pin, GPIO_PIN_SET);
HAL_Delay(100);
if (hal_status != HAL_OK) {
printf("HAL SPI TransmitReceive error: %d\r\n", (int) hal_status);
}
}
// Send read command
if (timer_flag){
txInConvertData = ReadCommandMask | (255 << 8);
//txInConvertData = ConvertCommandMask | (0 << 8); // Converts Channel
HAL_GPIO_WritePin(IN_SPI2_CS_GPIO_Port, IN_SPI2_CS_Pin, GPIO_PIN_RESET);
hal_status = HAL_SPI_TransmitReceive(&hspi2, (uint8_t*) &txInConvertData, (uint8_t*) &rxInConvertData[j], 1, 100);
HAL_GPIO_WritePin(IN_SPI2_CS_GPIO_Port, IN_SPI2_CS_Pin, GPIO_PIN_SET);
//HAL_Delay(100);
if (hal_status != HAL_OK) {
printf("HAL SPI TransmitReceive error: %d\r\n", (int) hal_status);
}
j = j + 1;
//timer_flag = 0;
}
if (j == 20000){
HAL_TIM_Base_Stop_IT(&htim10);
j = 0;
timer_flag = 0;
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-10 9:33 AM
Do you have the TIM10 interrupt enabled in the "NVIC" tab of the timer config dialog in CubeMX?
Does your callback ever get called? Set a breakpoint and see.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-10 10:03 AM
Yes, it was enabled.
Yes, I placed a toggling command for a GPIO pin and it worked.