cancel
Showing results for 
Search instead for 
Did you mean: 

Correct names of STM32F407VGT6 ADCs?

karlis
Associate II
Posted on December 29, 2017 at 17:10

Hi everyone. I have kinda dumb question...

In reference manual and in libraries I am using I see that STM32F407VGT6 has ADC1, ADC2, and ADC3.

But when I check the ping definition table it shows ADC12, ADC123 and ADC3.

Can anyone help and tell my why they are called like that and not ADC1,2,3?

I am particulary interested in PB0 pin, which is input for ADC12_IN8...Which ADC is this?

Thanks in advance

#adc123 #adc1 #adc12 #stm32f40
1 REPLY 1
Posted on December 29, 2017 at 17:23

 ADC12_IN8

Channel 8 on ADC1 or ADC2

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..