2017-12-28 8:27 PM
Hi.
I'm trying to use
'Boot from Embedded SRAM mode' in KEIL MDK.
Where can I find reference example of 'Boot from Embedded SRAM mode' with STM32F103 ?
2017-12-29 7:10 AM
You probably won't 'find' an example, you should apply your knowledge of micro-processors and compilers/linkers to create one. Right now you're so far over your skis that you need to explain why this functionality is important for you to understand.
2017-12-29 7:14 AM
Perhaps there are some code example to boot STM32 by UART in the tool smt32flash.
This tool will boot SMT32 from SRAM after flash code
It's open-source,
http://stm32flash.sourceforge.net
from its help, The communication protocol used by ST bootloader is documented in following ST application notes
· AN3155: USART protocol used in the STM32(TM) bootloader
· AN4221: I2C protocol used in the STM32 bootloader
HTH
2017-12-29 8:21 AM
I can't understand why everybody wants to know what why I have this question, I want to ask you vice-versa.
2017-12-29 8:23 AM
Thanks Chen.
2017-12-29 8:30 AM
After search, perhaps I got wrong because that tool is to boot STM32 from 'User Flash', 'boot from embedeed SRAM' is totally different thing. Please forget my post!