2017-12-29 8:10 AM
Hi everyone. I have kinda dumb question...
In reference manual and in libraries I am using I see that STM32F407VGT6 has ADC1, ADC2, and ADC3.
But when I check the ping definition table it shows ADC12, ADC123 and ADC3.
Can anyone help and tell my why they are called like that and not ADC1,2,3?
I am particulary interested in PB0 pin, which is input for ADC12_IN8...Which ADC is this?
Thanks in advance
#adc123 #adc1 #adc12 #stm32f402017-12-29 8:23 AM
ADC12_IN8
Channel 8 on ADC1 or ADC2