2017-05-05 09:44 AM
Hi,
I'm trying to connect a TTL-232R USB-UART Converter to an STM32F3DISCOVERY board. I've connected the TX/RX wires on the TTL-232R to PB10/PB11 on the STM32F3DISCOVERY board. I have the board connected to my laptop over USB.
Do I need to connect the 5V/GND wires on the TTL-232R? Or are these signals already provided by USB?
Any help would be much appreciated.
Cheers,
Tony
#uart #stm32f3-discoverySolved! Go to Solution.
2017-05-09 10:05 AM
Yes my mistake, I've fixed this and connected TX to RX
2017-05-09 10:06 AM
Thanks for your help Edison, I've resolved this problem