2024-12-11 12:09 PM - last edited on 2024-12-17 1:45 PM by Tesla DeLorean
I am a newborn to this whole side of tech
I am running Windows 11
I have bluepill that I am trying to run the bluepill diagnostics from
https://mecrisp-stellaris-folkdoc.sourceforge.io/bluepill-diags-v1.640.html#bluepill-diags-v1-640
I am using a STLINKv2 USB clone and flashed the bluepill diagnostics to the bluepill
I am now attempting to connect to the bluepill to run the diagnostics
Initially I tried to use the connection via the STLinkv2 adapter but do not see a new COM port for it (Intel Active MGMT is COM3)
I then thought the mini-usb may be where I need to connect to but also with no joy in connecting or seeing a new COM port
Any idea what I am missing
Solved! Go to Solution.
2024-12-17 1:35 PM
https://community.st.com/t5/stm32-mcus-products/confirm-genuine-or-fake-bluepill-board/td-p/754612
You could write simple test code to blink an LED.
You could buy a NUCLEO board, and save a lot of your own time, if that's worth anything.
2024-12-18 12:42 AM
@Tesla DeLorean wrote:You could buy a NUCLEO board, and save a lot of your own time
Absolutely!
And a Nucleo board would include a genuine ST-Link.
@xq1xq1xq1 especially as you say you are "a newborn to this whole side of tech" you would make your life a whole lot easier using genuine, supported products and tools.
Get to know how the products & tools should work before trying to debug questionable parts!
See this for some example tales of woe resulting from the bluepill fakery:
2024-12-18 3:50 PM
I didn't know about nucleo
The project I'm working on requires a bluepill stm32f10 in a similar or smaller footprint.
I did a search and only seemed to find L432 type chips on nucleo
Any source for an equivalent stm32f10 chip is appreciated.
2024-12-18 3:54 PM
I wrote a blink test that someone had given a guide on.
The led comes on but does not blink.
I'm unsure if this proves a fake chip or an error on my part
2024-12-18 4:13 PM
You may attach the code here using <> and attach the .ioc file. We can check it. Alternatively you can connect it to Arduino ide and programme it.
2024-12-19 2:28 AM - edited 2024-12-19 2:29 AM
@xq1xq1xq1 wrote:The project I'm working on requires a bluepill stm32f10 in a similar or smaller footprint
Even so, the recommendation is that you should start on a Nucleo board - to gain basic experience & understanding of how the chip and the tools should work.
At the moment, your struggles are hampered by not having those basics - and compounded by the unknown and unsupported hardware.
The smallest Nucleo is the Nucleo-32:
https://www.st.com/en/evaluation-tools/stm32-nucleo-boards.html
that looks about the same size as your "pill"?
2024-12-19 3:37 AM
Thanks for your guidance. I'll work towards that.