Skip to main content
Associate II
December 11, 2024
Solved

Connecting to BluePill via Serial Port

  • December 11, 2024
  • 5 replies
  • 4652 views

I am a newborn to this whole side of tech

I am running Windows 11

I have bluepill that I am trying to run the bluepill diagnostics from

https://mecrisp-stellaris-folkdoc.sourceforge.io/bluepill-diags-v1.640.html#bluepill-diags-v1-640

I am using a STLINKv2 USB clone and flashed the bluepill diagnostics to the bluepill

I am now attempting to connect to the bluepill to run the diagnostics

Initially I tried to use the connection via the STLinkv2 adapter but do not see a new COM port for it (Intel Active MGMT is COM3)

I then thought the mini-usb may be where I need to connect to but also with no joy in connecting or seeing a new COM port

Any idea what I am missing

Best answer by xq1xq1xq1

Thanks for your guidance. I'll work towards that. 

5 replies

Tesla DeLorean
Guru
December 11, 2024

It looks like that software should present as a USB CDC device, provided the BOOT jumpers are set to run the FLASH software

Should present in Device Manager as "Mecrisp STM32F10x Forth Serial Port" instead of "STM32 BOOT DEVICE" from the System Boot Loader. Check if it finds a device, or needs drivers

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
xq1xq1xq1Author
Associate II
December 11, 2024


I left the boot0 and boot1 jumpers on 0.

Do I need to make a change on the board?

Thx

Senior III
December 12, 2024

Techn_0-1734011714608.png

First you have to load the new firmware using st-link v2. Then select main flash memory option and plug the board into usb. Check device manager and let us know what does your windows device manager shows. Once the device manager is showing the board, using any serial monitor app to connect to that device as serial. Follow the steps given in the pdf file which is got in the zip folder.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Karl Yamashita
Principal
December 11, 2024

 

Maybe you have a Chinese knockoff of the BluePill? 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
xq1xq1xq1Author
Associate II
December 11, 2024

I was wondering if it is fake 

 
When I looked at the board in the stmprogrammer I got this:
 
Device ID: The Device ID 0x410 corresponds to the STM32F103C8T6, which is the chip used in the BluePill board.
 
Flash Size: The reported flash size is 128k, which matches the expected flash size for the STM32F103C8T6.
 
CPU: The Cortex-M3 core is correct for the STM32F103C8T6
 
Is there something else that I can do to verify if it's genuine or not? 
xq1xq1xq1Author
Associate II
December 16, 2024

If I understood you correctly, I left Boot0 and Boot1 on 0 to run flash memory.

I flashed the 

I disconnected the STLinkv2 USB Adapter and I connected the bluepill mini-usb to the computer and the power LED lights up.

BluePill_USB.jpg

I still only see the Intel COM Port in Device Manager

Device Manager Ports.jpg

I apologize if I am being dense, any ideas?

Tesla DeLorean
Guru
December 16, 2024

Would need bluepill-diagnostics-v1.6xx.bin successfully written to the STM32F103

You would expect the Windows ding-dong sounds if the device registers as a USB Device, and then would appear as something in Device Manager, either what you want, or as an "Unknown Device"

The functionality of the third-party software would be under the purview of the developer, not ST

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
xq1xq1xq1Author
Associate II
December 17, 2024

Thanks so much for confirming your experience with the diagnostic firmware. I will table my work with the diagnostic firmware for now. The author suggested using SWDCOM instead of a serial connection. I had trouble compiling and getting SWDCOM to execute on debian. 

I'm trying confirm whether or not my bluepill board is genuine or fake as my project is not behaving as I expect. 

Do you have any suggestions on how to confirm if my chip is genuine or not? 

Tesla DeLorean
Guru
December 17, 2024

https://community.st.com/t5/stm32-mcus-products/confirm-genuine-or-fake-bluepill-board/td-p/754612

You could write simple test code to blink an LED.

You could buy a NUCLEO board, and save a lot of your own time, if that's worth anything.

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Super User
December 18, 2024

@Tesla DeLorean wrote:

You could buy a NUCLEO board, and save a lot of your own time


Absolutely!

And a Nucleo board would include a genuine ST-Link.

@xq1xq1xq1 especially as you say you are "a newborn to this whole side of tech" you would make your life a whole lot easier using genuine, supported products and tools.

Get to know how the products & tools should work before trying to debug questionable parts!

See this for some example tales of woe resulting from the bluepill fakery:

https://community.st.com/t5/stm32-mcus-products/configuring-uart-on-stm32f103c8t6-bluepill-kills-connection-to/m-p/668641/highlight/true#M242690

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
xq1xq1xq1Author
Associate II
December 18, 2024

I didn't know about nucleo 

The project I'm working on requires a bluepill stm32f10 in a similar or smaller footprint. 

I did a search and only seemed to find L432 type chips on nucleo 

Any source for an equivalent stm32f10 chip is appreciated.