2024-07-03 01:39 AM - edited 2024-07-03 01:46 AM
Hello,
For my project I am working on two nucleo board H743ZI2.
Unfortunately, during an experimentation one of the boards ceased working (LD4 and LD6 red). Maybe a short circuit, I don't know.
Anyway I tried to purchase a new NUCLEO-H743ZI2 but it seems the production has stopped, some websites suggest H753ZI.
I cannot see anywhere a page which explains the difference bewteen those two models.
The page NUCLEO-H753ZI - STM32 Nucleo-144 development board with STM32H753ZI MCU, supports Arduino, ST Zio and morpho connectivity - STMicroelectronics seems to show the same features.
One datasheet shows this:
NUCLEO-H743ZI2
Ethernet
• USB OTG FS on Micro-AB connector
• STLINK-V3E
• LQFP144
NUCLEO-H753ZI
Ethernet
• USB OTG FS on Micro-AB connector
• STLINK-V3E
• Cryptography
• LQFP144
Question 1:
Is there a page that lists all the difference between NUCLEO-H743ZI2 and NUCLEO-H753ZI ?
Is there something else than the cryptography ?
Question 2:
Is it possible to use the same project one the Cube IDE for those two different boards ?
I would like to avoir having two different projects for two different cards.
Question 3:
If I need to create new project for NUCLEO-H753ZI, is there a simple way to import from NUCLEO-H743ZI2 ?
Or should i copy paste my source files one by one ?
Thank you
Solved! Go to Solution.
2024-07-03 04:26 AM
Hello @Kévin
1- The Only difference Between Both Boards (and MCUs) is just the Crypto part.
2- The Project created and work for the NUCLEO-H743ZI2 can be uploaded and works to a NUCLEO-H753ZI directly no need for modifications.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-03 04:26 AM
Hello @Kévin
1- The Only difference Between Both Boards (and MCUs) is just the Crypto part.
2- The Project created and work for the NUCLEO-H743ZI2 can be uploaded and works to a NUCLEO-H753ZI directly no need for modifications.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-03 04:34 AM
Thank you for the answer, I will try to directly upload the same project on the new card and hope it works !