cancel
Showing results for 
Search instead for 
Did you mean: 

Change system clock stm32f0 manual

hazall
Associate III

I want to change system clock as a PLL(using HSE) 20 Minute after systemInit. thats why I must change it in main function not system_stm32f0.c file.

Here is my code, Not working properly. I dint do anything interrupt function.

void ClockInit(void)

{

if ((RCC->CFGR & RCC_CFGR_SWS) == RCC_CFGR_SWS_PLL)

RCC->CFGR &= (uint32_t) (~RCC_CFGR_SW);

while ((RCC->CFGR & RCC_CFGR_SWS) != RCC_CFGR_SWS_HSI) {}

}

RCC->CR &= (uint32_t)(~RCC_CR_PLLON); 

while((RCC->CR & RCC_CR_PLLRDY) != 0) {}

RCC->CFGR &= ~(RCC_CFGR_PLLMULL | RCC_CFGR_PLLSRC);

  RCC->CFGR |= (uint32_t)(RCC_CFGR_PLLSRC_HSI_Div2 | RCC_CFGR_PLLMUL5);

 //RCC_PLLConfig(RCC_CFGR_PLLSRC_HSI_Div2,RCC_CFGR_PLLMUL5);

RCC->CR |= RCC_CR_PLLON; /* (7) */

while((RCC->CR & RCC_CR_PLLRDY) == 0) {}

RCC->CFGR |= (uint32_t) (RCC_CFGR_SW_PLL);

while ((RCC->CFGR & RCC_CFGR_SWS) != RCC_CFGR_SWS_PLL) {}

 SystemCoreClockUpdate();

}

Thanks for everything

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
waclawek.jan
Super User

What are exactly the symptoms?

Code looks good. Can't you single-step and observe the registers?

Which STM32? The 'F0 family has two different RCC setup (PLL prescaler).

JW

Piranha
Chief II

Did you adjusted the FLASH latency and APB prescalers properly before increasing the SYSCLK?

STM32F030C8T6TR

I changed code like that, it seems good

void RCC_HSE_Configuration(void){

RCC_DeInit();

RCC_HSEConfig(RCC_HSE_ON);

if(RCC_WaitForHSEStartUp() == SUCCESS){

RCC_HCLKConfig(RCC_SYSCLK_Div1);

RCC_PLLConfig(RCC_PLLSource_PREDIV1, RCC_PLLMul_4);  

RCC_PLLCmd(ENABLE);

while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET);

RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);

while(RCC_GetSYSCLKSource() != 0x08); 

}

SystemCoreClockUpdate();

}

No, I don't quite understand, can you show an example code?

Reference manual has an explanation and even exact sequences of actions listed.