cancel
Showing results for 
Search instead for 
Did you mean: 

CAN TX

Ash1
Associate III

Hi all

Can You provide me a correct code for how we can transfer TX frame using HAL .

please check my code below .

Issue what I am facing in my code is only I am seeing first ID data even data and ID are correctly stored inside buffer.

Please guide me .

PFA

18 REPLIES 18
Ash1
Associate III

Hi 

As I am unable to attached all images. I am replying on same post.

B.R

Ashish

Peter BENSCH
ST Employee

It's a bad idea to insert code as screenshots, partly because you can't search images for text.

There are therefore instructions in the Community Guidelines on how to insert code, for which there is an explicit function field </>, which you have also used in previous posts. Please remove the images and replace them with the code block.

Thank you
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SofLit
ST Employee

Hello,

Your description is not clear. See: https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

Also instead of attaching screenshots of your code, please use </> button to paste it here.

See: https://community.st.com/t5/community-guidelines/how-to-insert-source-code/ta-p/693413

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
Ash1
Associate III

Hi 

I am editing in the same post 

Please check code. I am getting HAL_OK every time but unable to see TI1R data on the BUS.ONLY TI0R data I can see. even transmit mail box value getting change alternative 0 to 1 still facing the issue

	while (1)
	{


		// Example: Transmit a CAN message
		CAN_TxHeaderTypeDef txHeader;
	 	const uint8_t tx_data[8] = {0x11};
		const uint8_t tx_data1[8] = {0x12};
		uint32_t tx_mailbox_used;

		txHeader.StdId = 0x3e8; // Example CAN ID
		txHeader.RTR = CAN_RTR_DATA;
		txHeader.IDE = CAN_ID_STD;
		txHeader.DLC = 8;

		if (HAL_CAN_AddTxMessage(&hcan1, &txHeader, tx_data, &tx_mailbox_used) != HAL_OK)
		{
			Error_Handler();
		}

		txHeader.StdId = 0x244; // Example CAN ID
				txHeader.RTR = CAN_RTR_DATA;
				txHeader.IDE = CAN_ID_STD;
				txHeader.DLC = 8;

		if (HAL_CAN_AddTxMessage(&hcan1, &txHeader, tx_data1, &tx_mailbox_used) != HAL_OK)
				{
					Error_Handler();
				}

		HAL_Delay(10);


	}







HAL_StatusTypeDef HAL_CAN_AddTxMessage(CAN_HandleTypeDef *hcan, const CAN_TxHeaderTypeDef *pHeader,
                                       const uint8_t aData[], uint32_t *pTxMailbox)
{
  uint32_t transmitmailbox;
  HAL_CAN_StateTypeDef state = hcan->State;
  uint32_t tsr = READ_REG(hcan->Instance->TSR);

  /* Check the parameters */
  assert_param(IS_CAN_IDTYPE(pHeader->IDE));
  assert_param(IS_CAN_RTR(pHeader->RTR));
  assert_param(IS_CAN_DLC(pHeader->DLC));
  if (pHeader->IDE == CAN_ID_STD)
  {
    assert_param(IS_CAN_STDID(pHeader->StdId));
  }
  else
  {
    assert_param(IS_CAN_EXTID(pHeader->ExtId));
  }
  assert_param(IS_FUNCTIONAL_STATE(pHeader->TransmitGlobalTime));

  if ((state == HAL_CAN_STATE_READY) ||
      (state == HAL_CAN_STATE_LISTENING))
  {
    /* Check that all the Tx mailboxes are not full */
    if (((tsr & CAN_TSR_TME0) != 0U) ||
        ((tsr & CAN_TSR_TME1) != 0U) ||
        ((tsr & CAN_TSR_TME2) != 0U))
    {
      /* Select an empty transmit mailbox */
      transmitmailbox = (tsr & CAN_TSR_CODE) >> CAN_TSR_CODE_Pos;

      /* Store the Tx mailbox */
      *pTxMailbox = (uint32_t)1 << transmitmailbox;

      /* Set up the Id */
      if (pHeader->IDE == CAN_ID_STD)
      {
        hcan->Instance->sTxMailBox[transmitmailbox].TIR = ((pHeader->StdId << CAN_TI0R_STID_Pos) |
                                                       pHeader->RTR);
      }
      else
      {
        hcan->Instance->sTxMailBox[transmitmailbox].TIR = ((pHeader->ExtId << CAN_TI0R_EXID_Pos) |
                                                           pHeader->IDE |
                                                           pHeader->RTR);
      }

      /* Set up the DLC */
      hcan->Instance->sTxMailBox[transmitmailbox].TDTR = (pHeader->DLC);

      /* Set up the Transmit Global Time mode */
      if (pHeader->TransmitGlobalTime == ENABLE)
      {
        SET_BIT(hcan->Instance->sTxMailBox[transmitmailbox].TDTR, CAN_TDT0R_TGT);
      }

      /* Set up the data field */
      WRITE_REG(hcan->Instance->sTxMailBox[transmitmailbox].TDHR,
                ((uint32_t)aData[7] << CAN_TDH0R_DATA7_Pos) |
                ((uint32_t)aData[6] << CAN_TDH0R_DATA6_Pos) |
                ((uint32_t)aData[5] << CAN_TDH0R_DATA5_Pos) |
                ((uint32_t)aData[4] << CAN_TDH0R_DATA4_Pos));
      WRITE_REG(hcan->Instance->sTxMailBox[transmitmailbox].TDLR,
                ((uint32_t)aData[3] << CAN_TDL0R_DATA3_Pos) |
                ((uint32_t)aData[2] << CAN_TDL0R_DATA2_Pos) |
                ((uint32_t)aData[1] << CAN_TDL0R_DATA1_Pos) |
                ((uint32_t)aData[0] << CAN_TDL0R_DATA0_Pos));

      /* Request transmission */
      SET_BIT(hcan->Instance->sTxMailBox[transmitmailbox].TIR, CAN_TI0R_TXRQ);



      /* Return function status */
      return HAL_OK;
    }
    else
    {
      /* Update error code */
      hcan->ErrorCode |= HAL_CAN_ERROR_PARAM;

      return HAL_ERROR;
    }
  }
  else
  {
    /* Update error code */
    hcan->ErrorCode |= HAL_CAN_ERROR_NOT_INITIALIZED;

    return HAL_ERROR;
  }
}

  

1- Please give more details about your HW. You are not even giving the MCU part number? the board? Which transceiver?

2- Are you using Normal or Loopback mode. Better to attach your project.

3- Your description still not clear. Which ID is not sent on the bus?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
Ash1
Associate III

Hi Sir

I am using STM32F407evb

2.I am using normal mode .

3. I have tried to send ID:3e8  data is (ox11) and ID:244 data(0x12) but I can see both ID transmitted at 10 ms but for both ID it is showing 0x11 only.   even data is stored correctly inside both tx buffers.

so please guide me how can I send multiple ID .

I tried sending one ID it is working fine but more than one is not working .

B.R

Ashish

I don't see any issue in your code you need to have both frames received:

ID: 0x3E8 with data 0x11 and ID: 244 with data 0x12.

Check your receiver.

Or use Loopback mode and receive what you are sending. If you are receiving well both frame, this means you have an issue with your receiver..

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
Ash1
Associate III

Hi

Okay I will try loopback mode and check .

Can it be issue because of clock .how much clock we should give atleast I am running 40mhz and 6 prescaler

Ash1
Associate III

Hi

Can you suggest me a example for LOOPback mode