2021-05-09 07:07 PM
I read the datasheet, a = device generation a, but I don't know what the difference is. Can you explain it in detail?
Solved! Go to Solution.
2021-05-10 02:55 AM
Hello @ZJian.2,
Let me first welcome you to the STM32 Community =)
I attached the Excel file detailing and comparing the characteristics of STM32L152C8Tx with STM32L152C8TxA.
The difference is on RAM:
You can use the ST-MCU-FINDER tool (integrated also in STM32CubeMX) which offers the features to compare the characteristics of two or more MCUs through the "Cross Selector" tab. I advise you to refer to the UM1718 in section "Cross selector" for more details.
When your question is answered, please close this topic by choosing "Select as Best". This will help other users find that answer faster :smiling_face_with_smiling_eyes:.
Imen
2021-05-09 07:59 PM
Guess you'd want to look at the Reference Manual and DEV_ID, and then the Errata, which should indicate the types of things fixed in later steppings of the IC
2021-05-09 08:44 PM
Sorry,I don't know what you're talking about. You seem to offer a way, but that's not what I want to ask for.
2021-05-10 02:55 AM
Hello @ZJian.2,
Let me first welcome you to the STM32 Community =)
I attached the Excel file detailing and comparing the characteristics of STM32L152C8Tx with STM32L152C8TxA.
The difference is on RAM:
You can use the ST-MCU-FINDER tool (integrated also in STM32CubeMX) which offers the features to compare the characteristics of two or more MCUs through the "Cross Selector" tab. I advise you to refer to the UM1718 in section "Cross selector" for more details.
When your question is answered, please close this topic by choosing "Select as Best". This will help other users find that answer faster :smiling_face_with_smiling_eyes:.
Imen
2021-05-10 03:23 AM
There's also a migration document between the non-suffixed and -A-suffixed STM32L15x, TN1176.
JW