2024-11-28 02:25 AM
#include "Main.h"
#define MAX_Intensity 1600
static volatile uint16_t Intensity = 10;
void Timer4_Configuration(void)
{
TIM_TimeBaseInitTypeDef TIM_BaseStructure;
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE);
TIM_BaseStructure.TIM_Prescaler = 1 - 1;
TIM_BaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_BaseStructure.TIM_Period = MAX_Intensity - 1;
TIM_BaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_TimeBaseInit(TIM4, &TIM_BaseStructure);
TIM_Cmd(TIM4, ENABLE);
}
void PWM_Configuration()
{
TIM_OCInitTypeDef TIM_OCStructure;
TIM_OCStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OCStructure.TIM_Pulse = 0;
TIM_OC1Init(TIM4, &TIM_OCStructure);
TIM_OC1PreloadConfig(TIM4, TIM_OCPreload_Enable);
TIM_OC2Init(TIM4, &TIM_OCStructure);
TIM_OC2PreloadConfig(TIM4, TIM_OCPreload_Enable);
TIM_OC3Init(TIM4, &TIM_OCStructure);
TIM_OC3PreloadConfig(TIM4, TIM_OCPreload_Enable);
TIM_OC4Init(TIM4, &TIM_OCStructure);
TIM_OC4PreloadConfig(TIM4, TIM_OCPreload_Enable);
}
void GPIO_PWM_Configuration()
{
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource12, GPIO_AF_TIM4);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource13, GPIO_AF_TIM4);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource14, GPIO_AF_TIM4);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource15, GPIO_AF_TIM4);
GPIO_InitStructure.GPIO_Pin = ALL_LEDS;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOD, &GPIO_InitStructure);
}
void TIM2_Configuration(u32 Intervalms)
{
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_TimeBaseStructure.TIM_Prescaler = 16000-1;
TIM_TimeBaseStructure.TIM_Period = Intervalms-1;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE);
TIM_Cmd(TIM2, ENABLE);
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1);
NVIC_InitTypeDef NVIC_InitStructure;
NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
int main(void)
{
GPIO_PWM_Configuration();
Timer4_Configuration();
PWM_Configuration();
TIM2_Configuration(500);
while(1)
{
}
}
void TIM2_IRQHandler()
{
if(TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET)
{
if(Intensity > MAX_Intensity)
{
Intensity = 10;
}
TIM4->CCR1 = Intensity;
TIM4->CCR2 = Intensity;
TIM4->CCR3 = Intensity;
TIM4->CCR4 = Intensity;
Intensity = Intensity * 2;
TIM_ClearITPendingBit(TIM2, TIM_IT_Update);
}
}
The code above is the example I am referring to. However, the Timer2 interrupt does not occur in this code. However, if you change the Timer2Configuration function call to before the PWM_Configuration function call, the interrupt operates normally. I can't find the cause of this behavior, so I'm asking a question.
i'm conducting practice using STM32F407G-DISC1.
2024-11-28 03:08 AM
Hello @treeset, welcome to ST community,
I think that the part in the TIM2 configuration that makes it work is the NVIC configuration, it's mandatory to configure the NVIC before enabling interrupts
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-28 04:06 AM
int main(void)
{
GPIO_PWM_Configuration();
TIM2_Configuration(500);
Timer4_Configuration();
PWM_Configuration();
while(1)
{
}
}
Try like this.