2024-07-18 04:39 AM - last edited on 2024-07-18 04:43 AM by SofLit
I am trying to interface CAN communication in loopback mode in STM32F469I DISCO but it is not working.
2024-07-18 04:42 AM
Hello @jrupesh90_ and welcome to the community.
You need to describe what kind of issue you are facing.
You can refer to this link on how to post a thread.
You need to share your project including the ioc file.
2024-07-18 04:53 AM
I am trying to interface CAN in loopback mode in STM32F469I DISCO board but my code is not working. Can you provide me some code snippets with respect to board.
2024-07-18 04:58 AM - edited 2024-07-18 05:00 AM
There is no CAN examples available for STM32F469I DISCO board but you can inspire from the example provided in the STM32CubeF4 in github from this link for STM32469I_EVAL board (the same microcontroller, but you need to check the RCC and the CAN GPIO pins configurations):
But you didn't share your code to look at it.
Two questions:
Did you enable and configure correctly the filters.
Did you configure the internal pull-up resistor for CAN_Tx pin ?