2020-05-22 08:42 PM
2020-05-23 03:45 AM
2020-05-22 10:59 PM
Which STM32 in particular?
Is there anything related mentioned in the errata?
JW
2020-05-23 01:10 AM
Thanks.
It is a STM32H743IIT6. ( - VQ911426 AA157 - TWN AK 936 - V e3)
Looks like the silicon is Revision V, manufactured in 36s week of 2019.
The latest RM0433 still says the pins can be used as GPIO if the DAC is configured to connect to internal parts only.
Frank
2020-05-23 03:45 AM
JW
2020-05-23 03:55 AM
Thanks