Can I get source code of low power mode for STM32F413 series micro-controller ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-09-05 7:30 AM
I want to integrate low power mode application in my project code so following things I tried so far, please do attention and help me out..,
I have source code of PWR Current Consumption example from different series (STM32F407xx devices) got it from IDE repository.
I have create new project and made proper board configuration settings according to my discovery board what I have ie., STM32F413 HT6 and integrated PWR Current Consumption example code (STM32F407xx devices). which is different series. Once I flash this integrated code in my board it causing ST-LINK DLL error/error in final launch sequence (board loosing its hardware integrity) means failed to flash so that I need to make boot 0 pin up and flash . repeatedly i am facing error because of SleepMode_Measure() function init.
If any one worked with low power mode for STM32F413 discovery kit please share with me or how to resolve with existing code(STM32F407xx devices).
Regards,
Nitish
- Labels:
-
Power
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-09-05 8:06 AM
Unsurprisingly when you remove power from the debug interface it stops working.
For low power testing/reporting you should perhaps provide telemetry via a UART and VCP, indicating when you power up/down.
Have your device enter low power modes in a more controller fashion, ie from a button press, or UART interaction, this way the debugger won't die immediately as it typically has to allow the code to execute and break-point it to stop, and this might take several thousand cycles. Also look at "Connect Under Reset" options.
Perhaps look at these examples as starting points
STM32Cube_FW_F4_V1.24.1\Projects\STM32F413ZH-Nucleo\Examples\PWR
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-09-06 3:38 AM
Thanks for immediate response..,
Yes, debugger won't die immediately until it was working from button pressed but I am flashing and checking it through multi meter whether it is entering into low power or not through debugger cable . Is it way of checking power ? or is there any way to check power up/down and can you please elaborate connection of "telemetry via UART and VCP" it may help me to test further
I am using STM32F413 Discovery board, is that STM32F413ZH-Nucleo board source will work for my board? or is any changes should I make to test, please correct me if I am wrong.
Regards,
Nitish