Skip to main content
Associate II
April 15, 2025
Question

Optimizing ILI9488 SPI Display Performance with STM32G0B0VET6 – Too Slow?

  • April 15, 2025
  • 4 replies
  • 2203 views

Hi everyone,

I'm working on a project using the STM32G0B0VET6 microcontroller, and I have an ILI9488 TFT display (320x480) connected via SPI. There is no external display controller – the STM32 is driving the display directly.

Problem
The display works and renders correctly using custom drivers, but the refresh/update speed is very slow, especially when trying to render large bitmaps or full-screen updates. This is a major bottleneck in my application.

What I've Tried

  • Using SPI1 at the highest possible baud rate (around 24–27 MHz).
  • Optimizing HAL_SPI_Transmit() and buffering with DMA.
  • Rendering images with a tile-based approach to avoid RAM overflow (since STM32G0B0 has only 144KB RAM).
  • Converting and sending RGB565 bitmaps using a fast push function.
  • Even tried lower-resolution images scaled up – no significant improvement.

Questions

  • Is it realistically possible to achieve smooth full-screen updates with this MCU driving the ILI9488 directly over SPI?
  • Am I wasting time trying to optimize this on an STM32G0 series chip without external display control?
  • Has anyone had success with speeding up ILI9488 performance on low-power STM32s?
  • Any tips on improving SPI display throughput or managing full-screen rendering more efficiently would be appreciated.

Thanks in advance!

4 replies

Ozone
Principal
April 15, 2025

> I'm working on a project using the STM32G0B0VET6 microcontroller, and I have an ILI9488 TFT display (320x480) connected via SPI.

> .. using SPI1 at the highest possible baud rate (24-27 MHz)

That gives you 320 * 480 * 2 bytes to transfer, i.e. 307.200 bytes, or 2.457.600 bits total.
Even at 27 MBit/s, a full screen update requires almost a second - at best.


I would think your choice of MCU, display, and rendering/throughput requirements don't go well together.
One has to give.

RobK1
Associate II
April 15, 2025

Do you have the source code for the drivers you are using?

I have an application with an ILI9163V and the driver I found for that controller did not correctly use the windowing/auto-increment function of the controller. After correcting that, I had a ~20x improvement in update speed. 

alfsch
Associate
April 15, 2025

Hi,

what is " too slow" ?

(as @Ozone wrote ) you can expect only as a max. possible speed, what the SPI interface can write at the limit of the ILI chip : full screen write , cls , would be about 2.457.600 bits , at 24Mbit -> 100 ms , is absolute maximum you can reach - just from possilble speed of ILIxxx SPI interface.

Whats your speed now, for a "cls" , full screen fill ?

AldrinAuthor
Associate II
April 15, 2025

Too slow in the sense, even while using trying to print an image it take about more than 3 sec to fill the whole screen.

cls happens in less than a sec but still can be observed.

Ozone
Principal
April 15, 2025

You didn't mention the use case.

So, if these time requirements are not acceptable to the user, you could either use a smaller display, or choose a configuration which drives the display with a parallel interface.

With some knowledge of the MCU and the interfacing method, you can estimate the data throughput (required vs. delivered) accurately enough to check for your requirements.