2012-11-06 04:12 AM
Hi,
I was looking for an example of a CAN BUS for STM32F4 can you help?2012-11-06 07:05 AM
\STM32F4xx_DSP_StdPeriph_Lib_V1.0.1\Project\STM32F4xx_StdPeriph_Examples\CAN\LoopBack
2012-11-06 12:47 PM
:-D Thanks Clive, I saw that there are two examples, Loopback and Networking, networking as I understand it is the right one for me, because I have to communicate two evaluation boards STM32F4 discovery! very kind as always! :-)
2012-11-06 12:57 PM
Loopback has the demonstrable advantage of not requiring transceivers, or a bus, but the code changes required to actually transmit data are not particularly big.