Visitor II
November 5, 2012
Question
STM32 communicate with MIPI RFFE interface.
- 1 reply
- 1630 views
Posted on November 05, 2012 at 23:47
I am thining of to use STM32 to communicate with MIPI interface. Please see the typical format in the attachment. It is hard to do that with PIC18F controller, for data rate up to 26MHz; by-directional TX/RX SPI like data from 1 pin; 23 clocks's data for TX and 24 clocks's data for RX.
Can it be done on STM32? #23-is-prime