cancel
Showing results for 
Search instead for 
Did you mean: 

CAN BUS

orn
Associate II
Posted on November 06, 2012 at 13:12

Hi,

I was looking for an example of a CAN BUS for STM32F4 can you help?
3 REPLIES 3
Posted on November 06, 2012 at 16:05

\STM32F4xx_DSP_StdPeriph_Lib_V1.0.1\Project\STM32F4xx_StdPeriph_Examples\CAN\LoopBack

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
orn
Associate II
Posted on November 06, 2012 at 21:47

:D Thanks Clive, I saw that there are two examples, Loopback and Networking, networking as I understand it is the right one for me, because I have to communicate two evaluation boards STM32F4 discovery! very kind as always! :)

Posted on November 06, 2012 at 21:57

Loopback has the demonstrable advantage of not requiring transceivers, or a bus, but the code changes required to actually transmit data are not particularly big.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..