2022-07-25 1:22 AM
Hi I'm trying to generate a signal with 100 ns time on and 100 ns time off thanks to DMA transfer. My problem is that I have a peak of tension before and I don't know what is it (F446RE)
Here is my code:
int main (void)
{
/*Clock and Power initialization*/
rccInit();
/*GPIO initialization*/
gpioInit();
/*External trigger initialization*/
externalTrigger();
/*Timers initialization*/
timInit();
/*DMA Initialization*/
dmaInit((uint32_t)buffer32b,longueurTotale);
GPIO
#include "stm32f4xx.h"
#include "gpio.h"
#define GPIOAEN (1U<<0)
#define PIN5 (1U<<5)
#define LED_PIN PIN5
#define AFR5_TIM (1U<<20)
void gpioInit(void)
{
RCC->AHB1ENR |=GPIOAEN; /* AHB1 clock enable*/
GPIOA->MODER |=(1U<<11); /*Mode alternate*/
GPIOA->MODER &=~(1U<<10);/*Mode alternate*/
GPIOA->PUPDR |=(1U<<10); /*Pull-Up*/
GPIOA->OSPEEDR|= ((1U<<10)|(1U<<11)); // Very High speed
GPIOA->AFR[0] |=AFR5_TIM; //Alternate function -> DATASHEET , enabling TIM2 CH1
}
Timer
#include "stm32f4xx.h"
#include "tim.h"
#define PW1 ((1<<6)|(1<<5))
#define Preload1 (1<<3)
#define autoReload (1<<7)
#define TIM2EN (1U<<0)
#define CR1_CEN (1U<<0)
#define TIM_DMA_UPDATE (1U<<8)
#define TIM2_DCR_DBL 0x00000200U // 3 DMA burst transfer and start from ARR register
#define TIM2_DCR_DBA 0x0000000BU
#define Fast (1U<<2)
#define DIER_UIE (1U<<0)
void timInit(void)
{
RCC->APB1ENR |=TIM2EN;
/*Set prescaler value*/
TIM2->PSC = 0 ;
TIM2->ARR = 0;
TIM2->CCR1= 0;
TIM2->CNT = 0;
TIM1->CR1 &= ~( TIM_CR1_DIR | TIM_CR1_CMS);
TIM1->CCMR1 &= ~TIM_CCMR1_OC1M;
TIM1->CCMR1 &= ~TIM_CCMR1_CC1S;
TIM2->CCMR1 |= (PW1 | Preload1 |Fast);
TIM2->CR1 |= autoReload;
TIM2-> DIER|= TIM_DMA_UPDATE;
//TIM2->DIER |=DIER_UIE;
TIM2->DCR &= ~TIM_DCR_DBA;
TIM2->DCR &= ~TIM_DCR_DBL;
TIM2-> DCR|= (TIM2_DCR_DBL | TIM2_DCR_DBA); // 3 DMA burst transfer and start from ARR register
TIM2-> EGR|= TIM_EGR_UG;
while((TIM2->EGR & TIM_EGR_UG) == SET){}
TIM2->EGR |= TIM_EGR_UG;
TIM2->BDTR|=TIM_BDTR_MOE;
TIM2->CCER |= TIM_CCER_CC1E;
TIM2->CR1 |=CR1_CEN;
//NVIC_EnableIRQ(TIM2_IRQn);
}
DMA
#include "stm32f4xx.h"
#include "dma.h"
#define RCC_AHB1ENR_DMA1_EN (1<<21) // Enable clock access to DMA1
#define DMA_PRIORITY_HIGH ((1<<17)|(1<<16)) // Very high priority
#define DMA_CIRCULAR (1<<8) // Circular mode
#define DMA_MEMORY_TO_PERIPH (1<<6) // DMA de la mémoire au périph
#define DMA_MINC_ENABLE (1<<10) //Incrémentation de la zone de mémoire
#define DMA_CHANNEL_3 ((1<<26)|(1<<25)) // Selection channel 3
#define DMA_MSIZE (1<<14) // Les données de mémoire sont de types word 32bits
#define DMA_PSIZE (1<<12) // Les données périphériques sont de types word 32bits
#define TIM2_DMAR_ADDRESS 0x4000004C
/******************* Bit definition for TIM_DMAR register *******************/
#define TIM_DMAR_DMAB_Pos (0U)
#define TIM_DMAR_DMAB_Msk (0xFFFFUL << TIM_DMAR_DMAB_Pos) /*!< 0x0000FFFF */
#define TIM_DMAR_DMAB TIM_DMAR_DMAB_Msk /*!<DMA register for burst accesses */
void dmaInit(uint32_t src, uint32_t data)
{
RCC->AHB1ENR |= RCC_AHB1ENR_DMA1_EN; // Enable clock access to DMA1
DMA1_Stream1->CR = 0;
DMA1_Stream1->CR |= (1<<4)|(1<<3)|(1<<2);
DMA1_Stream1->CR |= DMA_MEMORY_TO_PERIPH | DMA_MINC_ENABLE|DMA_CIRCULAR | DMA_PRIORITY_HIGH|DMA_CHANNEL_3|DMA_MSIZE|DMA_PSIZE;
DMA1_Stream1->NDTR = data;
DMA1_Stream1->PAR = (uint32_t)&TIM2->DMAR; // ARR Adress
DMA1_Stream1->M0AR = src;
NVIC_EnableIRQ(DMA1_Stream1_IRQn);
DMA1_Stream1->CR|= (1<<0);
// Manque l'autorisation des interruptions?
}
Solved! Go to Solution.
2022-07-27 6:24 AM
I found the problem -> set pin to no pull up no pull down and -> Enable alternate fucntion of pin and timers at the end of all initialisations
TIM2->CR1 |=CR1_CEN;
DMA1_Stream1->CR|= (1<<0);
GPIOA->AFR[0] |=AFR5_TIM;
2022-07-25 4:33 AM
Debug your code step by step with the scope connected and find which statement causes what behaviour.
Btw, I don't see a reason for using DMA for such a regular waveform, but you might have your reasons.
hth
KnarfB
2022-07-27 6:24 AM
I found the problem -> set pin to no pull up no pull down and -> Enable alternate fucntion of pin and timers at the end of all initialisations
TIM2->CR1 |=CR1_CEN;
DMA1_Stream1->CR|= (1<<0);
GPIOA->AFR[0] |=AFR5_TIM;