cancel
Showing results for 
Search instead for 
Did you mean: 

Boot Issue with CM4 - STM32H745ZIT6

Pavan-Oggu
Associate II

Hello Team,

We have a custom STM32H745 board designed and We are able to get the IC up and running on cube programmer and even set option bytes. 

The board is designed with Nucleo-H745ZI-Q schematics and we have verified everything on hardware end.

When we try to program the board with a basic blink sketch following the guide (https://www.st.com/resource/en/application_note/dm00629855-getting-started-with-projects-based-on-dualcore-stm32h7-microcontrollers-in-stm32cubeide-stmicroelectronics.pdf

M7 gets debugged and runs. Once I start with M4 I get error messages and it bricks the controller.

I have been pulling up the BOOT0 pin and performing mass erase and trying things again, still it gets bricked when I try to debug CM4.


13 REPLIES 13

We are using LDO mode and I can confirm that. I have attached our schematics for reference.

We have missed pull down resistor on boot0 but I have added it externally on the hardware, Similarly I have also added a pull up resistor for PDR_ON pin.

SofLit
ST Employee

Hello,

There is a mismatch between your RCC config i.e. you set an external 8MHz source in Bypass mode:

SofLit_0-1732788844117.png

 

While in your schematics you have an external clock with 25Mhz / Crystal/Resonator mode:

SofLit_1-1732788967663.png

You need to align the RCC config to fit your HW:

SofLit_0-1732789888616.png

SofLit_2-1732789105745.png

Attached the updated ioc file.

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Hello SofLit,

Thank you, CM7 boots up and blink sketch works on the board.
But CM4 remains the same. It doesn't get detected at all. Any idea why?

PavanOggu_0-1732796192832.png

 

Please comment these two lines in the main of CM4:

 

  HAL_PWREx_ClearPendingEvent();
  HAL_PWREx_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFE, PWR_D2_DOMAIN);

 

These lines make the CM4 to enter in low power mode while debugging.

For debug, I suggest you to comment these lines but you can keep them while in standalone.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.